AXIS#.IL.COGCOMPH.N

Description

AXIS#.IL.COGCOMPH.N can be used to read / write the frequency of the cogging compensation sine waves.

For a given position, the compensation is calculated as follows:

Versions

Action Version Notes
Implemented 02-14-02-000  

General Information

Type

Read/Write Array

Units

N/A

Range

0 to 255

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.COGCOMPH.N 0

50dch

01h

Unsigned8

-

-

Read/Write

No

AXIS1.IL.COGCOMPH.N 1

50dch

02h

Unsigned8

-

-

Read/Write

No

AXIS1.IL.COGCOMPH.N 2

50dch

03h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5868

1

5868 (0x16ec)

AXIS1.IL.COGCOMPH.N

Unsigned8[3]

Read/Write

Yes

71404

2

5868 (0x16ec)

AXIS2.IL.COGCOMPH.N

Unsigned8[3]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.COGCOMPH.N

5868

Unsigned8[3]

Read/Write

-